IMX219 driver on imx7d dual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX219 driver on imx7d dual

3,882件の閲覧回数
maitegonzalez
Contributor I

Hello,

I am trying to get frames from IMX219 cmos sensor. I have made the driver based on OV5657 soported driver.

I dont know sure how to configure the device tree, specially mipi_csi clock frecuency, csis-hs-settle,etc (I have attached).

When I try to capture a frame through v4l2 or gstreamer, the camera freezes on getting clock and nothing happens. (It seems there is any mipi_csi interrupt). 

I have attached the driver (It may be a little bit messy such as I have been testing different options)

Any ideas??

Thanks in advance,

Maite

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,855件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Maite

ov5647 is supported for i.MX7D:
drivers/media/platform/mxc/subdev/ov5647_mipi.c

IMX219 driver

Sony-IMX219-Raspberry-Pi-V2-CMOS/imx219mipiraw_Sensor.c at master · rellimmot/Sony-IMX219-Raspberry-... 

Debugging can be start with adjusting clocks:

https://community.nxp.com/docs/DOC-94312 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,077件の閲覧回数
dogisfat
Contributor IV

Were you able to get the sensor working with the imx7d?

0 件の賞賛
返信