IMX DUAL Lite and IS43TR16256A-125kbl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX DUAL Lite and IS43TR16256A-125kbl

571 Views
kbtess
Contributor II

Hi All,

We are developing a custom board using
IMX Dual Lite processor.

We are trying to use I GB (IS43TR16256A-
125KBL) memory.

But some of the the board fails
randomly  , even if I updated the MMDC
register after running the DDR stress test tool (2.52)

, Anybody succeeded in interfacing IS43TR16256A-
125KBL with Dual lite or any other processors ?

Tags (1)
0 Kudos
Reply
1 Reply

381 Views
igorpadykov
NXP Employee
NXP Employee

Hi binuthomas

DDR stress test tool does not stress all power supplies, for example

VDD_SOC_CAP, VDD_PU_CAP, as for example linux hd video

application. So one can check these and other power supplies with

oscilloscope.

One can try the following experiments to determine if it is a hardware

PCB issue. Hand solder 22uF capacitors directly under center of chip.

Solder on top of the 0402 chips.

Have software Increase voltages of ARM_CAP, SOC_CAP, PU_CAP.

Other test may be cooling/heating device - if this helps, that may point

to incorrect driver strength settings.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply