IMX AXI BUS ERROR, GPU hang

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX AXI BUS ERROR, GPU hang

3,989 Views
john_smith
Contributor II

Hello!

I'm trying to implement the hibernation mode on IMX6Q and Android, but I have some problems with resuming process. Sometimes the system works fine after resuming from hibernation, but more often there are errors like:

fence timeout on [d46b2b80] after 3000ms
objs:
--------------
viv timeline viv_sync
  pt signaled@32.406061
  pt active
  pt active
  pt active

viv timeline viv_sync
  pt signaled@284.728167
  pt signaled@284.894002

viv timeline viv_sync

fences:
--------------
[d595fe00] StrictModeFlash:0: signaled
  viv timeline_pt signaled@32.406061

[d46b2b80] viv sync_fence-5556: active
  viv timeline_pt active

[d4cae380] com.android.launcher/com.and:0: active
  viv timeline_pt active

[d5fb8280] viv sync_fence-5559: active
  viv timeline_pt active

[d5fb8900] viv sync_fence-5560: signaled
  viv timeline_pt signaled@284.728167

[d48e9100] viv sync_fence-5561: signaled
  viv timeline_pt signaled@284.894002

[galcore]: GPU[0] hang, automatic recovery.
[galcore]: recovery done
[galcore]: AXI BUS ERROR
GPU[0](ChipModel=0x2000 ChipRevision=0x5108):
**************************
***   GPU STATE DUMP   ***
**************************
  axi      = 0x00000151
  idle     = 0x7FFFFFFE
    FE not idle
  DMA address is constant, but state is changing:
    0x00000800
    0x00000000
  dmaLow   = 0x40000002
  dmaHigh  = 0x2607B0E0
  dmaState = 0x00000000
    command state       = 0 (PAR_IDLE_ST)
    command DMA state   = 0 (CMD_IDLE_ST)
    command fetch state = 0 (FET_IDLE_ST)
    DMA request state   = 0 (REQ_IDLE_ST)

....................

What can cause these errors?

Any ideas are welcome, thank you in advance )

Labels (3)
Tags (4)
11 Replies

2,296 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

please try latest linux bsps on below link, it have many "fence" gpu improvements described

in Release Notes

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,296 Views
john_smith
Contributor II

Hi, Igor!

We've migrated to SabreSD board from our custom board and now use the latest official sources. But nothing has changed - the problem is the same:

fence timeout on [d46b2b80] after 3000ms
objs:
--------------
viv timeline viv_sync
  pt signaled@32.406061
  pt active
  pt active
  pt active

 

 

viv timeline viv_sync
  pt signaled@284.728167
  pt signaled@284.894002

..........................................

0 Kudos

2,296 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos

2,296 Views
john_smith
Contributor II

I have no problems with launching the board, I have problems with hibernation process on it......

0 Kudos

2,296 Views
igorpadykov
NXP Employee
NXP Employee

what about linux, is it ok ?

0 Kudos

2,296 Views
john_smith
Contributor II

there are also problems on official linux - console doesn't work after resuming from hibernation.

0 Kudos

2,296 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

I am afraid "hibernation" is not supported in nxp official bsps,

one can check linux documentation (Linux Manual Chapter Low-level Power Management (PM) Driver)

in Doc packages on below link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i.... 

Best regards
igor

0 Kudos

2,296 Views
john_smith
Contributor II

Do you have any suggestions or advices for Android case?

0 Kudos

2,296 Views
john_smith
Contributor II

Yes, there are no problems with GPU on linux and the system works fine for a long time after waking up from hibernation.

0 Kudos

2,296 Views
john_smith
Contributor II

I've tried the demo images for Android from Freescale. The only thing I changed is enabling hibernation in kernel configuration. After that I boot the board and try to hibernate and get these errors again and again.

0 Kudos

779 Views
xiangkunkong
Contributor II

Hi, @john_smith 

Did you resolved this problem for Android?

0 Kudos