Hello,
My board is an Apalis IMX8 QM with an ixora 1.2 carrier board and i am using tdx-reference-multimedia-image.
I have a dual screen HDMI and LVDS (touch screen) together.
as two single-channel
Hello
I have an an Apalis IMX8 QM module with an ixora 1.2 carrier board .
I want to connect output to 2 panels LVDS at the same time as two single-channel lvds config.
Do you know LVDS can be used as two single-channel??
My DTS config as bellow:
&ldb2 { status = "okay"; lvds-channel@0 { fsl,data-mapping = "spwg"; fsl,data-width = <24>; status = "okay";//okay reg = <0>; port@1 { reg = <1>; lvds1_out: endpoint { remote-endpoint = <&panel_lvds_in>; }; }; }; lvds-channel@1 { fsl,data-mapping = "spwg"; fsl,data-width = <24>; status = "okay"; reg = <1>; port@1 { reg = <1>; lvds2_out: endpoint { remote-endpoint = <&panel2_lvds_in>; }; }; }; };
panel_lvds: panel-lvds {
compatible = "panel-lvds";
backlight = <&backlight>;
status = "okay";
port {
panel_lvds_in: endpoint {
remote-endpoint = <&lvds1_out>;
};
};
};
panel2_lvds: panel2-lvds {
compatible = "panel-lvds";
backlight = <&backlight>;
status = "okay";
port {
panel2_lvds_in: endpoint {
remote-endpoint = <&lvds2_out>;
};
};
};
Hi
You can refer this patch based on MEK :
Hello @Zhiming_Liu
Thank you for answering
I saw that ago,,but i want to config lvds out as tow single channel on it for example ldb1 !!
the patch is for dual-mode and split-mode,no single-mode!!
I dont want to config it on tow lvds ldb1 and ldb2!!
Do you know LVDS1 can be used as two single-channel??
Can you help me,it possible config lvds out as tow single channel ??
Thank you for your help
Do you know LVDS1 can be used as two single-channel??
-->No, we don't support this.
well if you check our Apalis IMX8MQ datasheet page 37 you will see the possible LVDS configuration.
We have customers with 3 singel lane LVDS running at the same time.
Hello @gohlke_tx
Thank you very much for answering!!
Please,have a look at The LVDS Block Diagram of NXP Imx.8 :
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/IMX8QM-LVDS-mirror-dual-mode-reference-p...
Single Mode
Single mode (LVDS panel connects to one channel) panel 1 and panel 2 can be different panels.
It seems ,There are 2 video stream to lvds out,only and we cant use 3 lvds single-lane Display!!
Can you explain more about that,how to running 3 singel lane LVDS at the same time??
Is there any sample DeviceTree or Link about that!!
Thank you for your help!!
Best regards,
Hello @Zhiming_Liu again,,,
Thank you
I got more confused, please help,i cant understand how is it possible!!
I ask this question from Toradex forum because im using Toradex apalis imx8qm module now,
https://community.toradex.com/t/lvds-dual-mode-configuration/18484/11?u=hhami
they said,its possible!!
But you said dont support that!!
Can you help me more!!
thank you