IMX 6D6A fail to boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX 6D6A fail to boot

408 次查看
Makabaka
Contributor II

Hi :

I made some boards using IMX6D6A(D version) and the boot mode was configured as external parallel Norflash , but one of the boards failed to boot.

 

Using serial download mode(boot mode[1:0]),  can debug in RAM mode, and read SRC_SBMR1 is 00000000, SRC_SBMR2 is 30000001.This is not the right value.

Test power supply, crystal oscillator is OK.The problem persisted after replaced a new CPU.

Could you please help to analyze the reasons for this phenomenon?

0 项奖励
1 回复

399 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ziv5

 

for SRC_SBMR1,2 wrong values one can check power-up sequence using

oscilloscope and try to prolong POR duration (just for test up to 1sec.), also

may be recommended to check both crystals (24MHz, 32.768KHz).

As reference please use IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

 

Best regards
igor

 

0 项奖励