Hi,
Our end application using CM-FX6 ( IMX6 Quad based COM form Compulab) requires display data to be pushed simultaneously in both 24 Bit LCD and HDMI interfaces, our software team is able to do this for anyone of the interface at a time,from our understanding from IMX6 datasheet Up to four interfaces may be active in parallel,hence request your support to meet our end requirement.
Regards,
Harish.S
hi
please do you do that? Is the problem solved?
thank you
when you boot up the board, try to use the command "echo 0 > /sys/class/graphics/fb2/blank"