IMX 6 Sabrelite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 6 Sabrelite

854 Views
vigneshp
Contributor I

Hi ,

I am currently facing some problems with mxc_v4l2_tvin.out test in IMX6Q sabrelite. My system configuration is as follows:

1. LTIB version : L3.0.35_4.1

2. Ubuntu 14.04

Problem:

I am interfacing adv7180 decoder to the sabrelite card through IPU0->CSI0, the drivers are loaded properly, then when i run mxc_v4l2_tvin test the output the output is also displayed on the screen; but after some time the output gets blank. So pls provide some suggestions to overcome the issue.

Regards,

Vignesh

Labels (2)
0 Kudos
Reply
1 Reply

778 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vignesh

please try to disable blanking

Disable screen blanking on i.MX6 running Yocto | NXP Community

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply