IMX.6 CSI0 Parallel restart issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX.6 CSI0 Parallel restart issue

1,030 Views
oliverlewis
Contributor I


Hi Experts,

I'm using mxc_v4l2_capture.c and have implemented my own v4l2 sensor driver for our bespoke camera IC and seemingly it works, a little. After a reboot I can capture video successfully. If I stop the capture and restart it, the HSync and VSync alignment appears to be out (or worse capturing on the wrong edges). Only power-cycling the camera will bring it back up again (until the first restart).

It does not appear to be an issue with the camera itself. I can scope the signals and their polarity and frequency does not change. I can keep the camera running, while the capture is stopped and restarted, and the same thing happens. It does appear to be an issue with the CSI0 drivers somewhere. I'm using the simplest capture tree possible (CSI0->MEM->my app) with no processing, sizing or rotation in-between.

I'm not sure where to start debugging. The CSI_SENS_CONF register appears consistent across re-starts (0x8C0B) and the CSI_ACT_FRM_SIZE is the same each time too (0xEF013F).

Any pointer to where I should start debugging this would be great.

Kind regards

- Oliver

Using linux-fslc 4.1.23-00328

===========

SOLVED, thank. Dodgy camera IC which lost it's internal reference when stopped.

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

916 Views
gusarambula
NXP TechSupport
NXP TechSupport

Thank you Oliver, for updating with the solution!

0 Kudos
Reply