IMX 28 ethernet don't work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX 28 ethernet don't work

902 次查看
Pedro_ng
Contributor I

Hello

I use the imx283 evk and i want to buil a linux image on a sd card with eth0.

But when i buil and run my kernel with this line:(noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait fec_mac=00:08:02:6B:A3:1A)

I can't have ethernet and the dmesg is eth0: no PHY found

ifconfig SIOcsifflags: no such device.

 

What can i do?

标记 (1)
0 项奖励
回复
0 回复数