IMX 28 ethernet don't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX 28 ethernet don't work

905件の閲覧回数
Pedro_ng
Contributor I

Hello

I use the imx283 evk and i want to buil a linux image on a sd card with eth0.

But when i buil and run my kernel with this line:(noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait fec_mac=00:08:02:6B:A3:1A)

I can't have ethernet and the dmesg is eth0: no PHY found

ifconfig SIOcsifflags: no such device.

 

What can i do?

タグ(1)
0 件の賞賛
返信
0 返答(返信)