IM.X35 no serial(console) input (3.11.1)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IM.X35 no serial(console) input (3.11.1)

ソリューションへジャンプ
1,739件の閲覧回数
maxvankessel
Contributor II

I'm using an I.MX35 SOC with the freescale linux mainline  (3.11.1).

I'm unable to receive any bytes from the serial input, the serial input/output (UART3) is connected to the console.

Someone an idea what is wrong?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,670件の閲覧回数
maxvankessel
Contributor II

Thanks,

Both Tx and Rx were configured for different pins.

Transmit was working (not configured), but receiver wasn't doing a thing.

Fixed the problem by changing the pins to the correct RS232 pins.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,671件の閲覧回数
maxvankessel
Contributor II

Thanks,

Both Tx and Rx were configured for different pins.

Transmit was working (not configured), but receiver wasn't doing a thing.

Fixed the problem by changing the pins to the correct RS232 pins.

0 件の賞賛
返信
1,670件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Does U-boot work? It would help if you could post your board file, boot logs, etc.

0 件の賞賛
返信
1,669件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Max,

I recommend you first to check the serial configurations, the speed is 115200 for example. And make sure if your board is working.

Best Regards

Dan

0 件の賞賛
返信