IEEE1588 of i.MX535, i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEEE1588 of i.MX535, i.MX6Q

1,981 Views
YanjunLuo
Contributor IV

Hi,

We have products using i.MX535 and i.MX6Q, now we want to use the IEEE1588, and has several questions about.

Does it have software stack we can get ?

Does it have the filter to remove jitter ?

Does it provide extracted clock ?

Regards,

Yanjun Luo.

Labels (3)
0 Kudos
Reply
2 Replies

1,745 Views
igorpadykov
NXP Employee
NXP Employee

HI Yanjun

for i.MX53 it is answered below

Re: Anyone using IEEE-1588 on QSB?

for i.MX6 please read attached Linux Manual

sect.46.4.3 How to Use the Stacks in Linux

L3.14.28_1.0.0_iMX6QDLS_BUNDLE  : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,745 Views
YanjunLuo
Contributor IV

Hi igor,

Thanks for your information, I think it works, but it doesn't support the filter.

Regards,

Yanjun Luo.

0 Kudos
Reply