IEEE_1588 /PTP hardware timestamping with imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEEE_1588 /PTP hardware timestamping with imx6q

863 Views
harshitupreti
Contributor I

Regarding enabling PTP timestamping functionality in imx6Q.

there are two drivers available for PTP in the 3.0.35 kernal:

1. PTP clock driver

2. FEC driver with FEC_1588.

The first driver is getting built as a module and is visible in lsmod.

But the /sys/class/ptp/... gives null result.

We are unable to test the second implementation, as no appilcation is available to test the same.

Please help,

a.To understand how to use the ptp clock driver and does it provide HW timestamping on imx6

b.how can we test the fec_1588 HW timestamping, is there a sample application to test it?

0 Kudos
1 Reply

442 Views
_at
Contributor III

Are you able to solve it?

Any help/response on above query appreciated?

0 Kudos