IEEE_1588 /PTP hardware timestamping with imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IEEE_1588 /PTP hardware timestamping with imx6q

1,137件の閲覧回数
harshitupreti
Contributor I

Regarding enabling PTP timestamping functionality in imx6Q.

there are two drivers available for PTP in the 3.0.35 kernal:

1. PTP clock driver

2. FEC driver with FEC_1588.

The first driver is getting built as a module and is visible in lsmod.

But the /sys/class/ptp/... gives null result.

We are unable to test the second implementation, as no appilcation is available to test the same.

Please help,

a.To understand how to use the ptp clock driver and does it provide HW timestamping on imx6

b.how can we test the fec_1588 HW timestamping, is there a sample application to test it?

0 件の賞賛
返信
1 返信

716件の閲覧回数
_at
Contributor III

Are you able to solve it?

Any help/response on above query appreciated?

0 件の賞賛
返信