IC viewing and encoding flows using a single CSI video stream on the i.MX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IC viewing and encoding flows using a single CSI video stream on the i.MX53

ソリューションへジャンプ
2,252件の閲覧回数
LeonCraven
Contributor II

Hi,

Is it possible to view and encode a single video stream from the CSI using the IC for different tasks (IC task time sharing)?

For viewing the IC is required for resizing PAL or NTSC to XGA resolution. For encoding the IC is required to convert the colour space from 4:2:2 to 4:2:0 YUV.

In section 45.4.5.2 it states that the IC can switch between tasks but it reads like the current frame is processed using one set of parameters, the parameters are changed, and the next frame is processed using the new parameters. This suggests that two input streams to the IC are required, otherwise the display would get every second frame and the VPU every other frame?

If it is possible to have one input and two output flows from the IC, is there an example of how to do this in Linux?

Regards,

Leon

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
2,079件の閲覧回数
Philip_FSL
Contributor IV

Hi Leon,

The parameter changing is transparent.  The CSC matrices are setup independently for each task in the IC.  As long as the IC is capable of handling both operations summed during one frame period you should be OK. 

Philip

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,080件の閲覧回数
Philip_FSL
Contributor IV

Hi Leon,

The parameter changing is transparent.  The CSC matrices are setup independently for each task in the IC.  As long as the IC is capable of handling both operations summed during one frame period you should be OK. 

Philip

0 件の賞賛
返信