I2S connections to ESAI0 or ESAI1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2S connections to ESAI0 or ESAI1

761 Views
pbain
Contributor III

Hi, I am trying to work out the pin mapping (if possible) to send I2S audio from ESAI0 or ESAI1 of the i.MX8QM.
We currently have the I2S slave connected to SAI1, but need this for another audio codec:
SAI1_TXC ----> I2S_CLK
SAI1_TXD ----> I2S_TXD
SAI1_TXFS ---> I2S_WC

Are these 3 I2S signals able to be mapped to ESAI0 or ESAI1 and if so what is the mapping?

Regards

Peter

Tags (3)
0 Kudos
Reply
1 Reply

687 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

sai mapping can be found in IOMUXD Chapter of Reference Manual,

which can be obtained in local marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply