I2S and PCM Audio on iMX6 Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2S and PCM Audio on iMX6 Dual

1,636 Views
stephenbarton
Contributor II

We are working on an iMX6 Dual design and have three audio peripherals to connect:

* An HDMI Receiver with MCLK, BCLK, LRCLK and DATA output signals

* An I2S Digital Microphone with BCLK and WS in, DATA out

* A Wi-Fi/BlueTooth IC with PCM_CLK, PCM_SYNC, PCM_IN and PCM_OUT signals

 

We will be running Android as the operating system.

Question is: any recommendations on the best way or ways to connect the above 11 signals to the four audio ports - AUD3 to AUD6 - on the iMX6 Dual?

Labels (2)
Tags (2)
0 Kudos
2 Replies

747 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stephen

one can check AN2628 Programming Audio Applications, basically it is valid for i.MX6 AUDMUX too

http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

747 Views
stephenbarton
Contributor II

Hi, Igor, thanks for the link to the App Note

- Stephen

0 Kudos