We are working on an iMX6 Dual design and have three audio peripherals to connect:
* An HDMI Receiver with MCLK, BCLK, LRCLK and DATA output signals
* An I2S Digital Microphone with BCLK and WS in, DATA out
* A Wi-Fi/BlueTooth IC with PCM_CLK, PCM_SYNC, PCM_IN and PCM_OUT signals
We will be running Android as the operating system.
Question is: any recommendations on the best way or ways to connect the above 11 signals to the four audio ports - AUD3 to AUD6 - on the iMX6 Dual?
Hi Stephen
one can check AN2628 Programming Audio Applications, basically it is valid for i.MX6 AUDMUX too
http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Igor, thanks for the link to the App Note
- Stephen