I2S/PCM setting in CYW4356

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2S/PCM setting in CYW4356

962件の閲覧回数
amit251291
Contributor IV

We are working with IMX8QM MEK board, running on Android 9  automotive and interfaced M.2 module which has CYW4356 chipset.  It uses BCM4354A2.1CX.hcd firmware.

After interfacing this module we came to know that HFP audio is not working , we could only hear the noise. But A2DP and AVRCP, PBAP are working fine.

We want to know default I2C and PCM settings which are done as the part of this firmware.

1) Could you please let us know these parameters ?

2) Also we would like to know if there are any commands or tool which we use to change bluetooth PCM settings.

 

We would like to generate CYW4356 BT firmware for IMX*QM MEK board. Please help here

how to set I2S/PCM parameter in CYW4356 | Cypress Developer Community 

ラベル(2)
2 返答(返信)

861件の閲覧回数
nxf54947
NXP Employee
NXP Employee

Hello amitpk‌,

My suggestion is to get in contact with NXP Professional Services (link below this comment), they are in charge of Android Auto development. I am afraid that I cannot give you more information since the i.MX 8M QM documentation haven't been made publicly available yet.  My apologies for the inconvenience.

ANDROID-AUTO: Software Technology for Android Auto

Best regards, 

Ruben

0 件の賞賛
返信

861件の閲覧回数
amit251291
Contributor IV

Thanks Ruben for your reply & suggestion. We will do the needful.