I2S Master mode with oversampling clock in kernel 3.10.17

cancel
Showing results for 
Search instead for 
Did you mean: 

I2S Master mode with oversampling clock in kernel 3.10.17

828 Views
dabrain
Contributor I

Hello,

I'm using a kernel 3.10.17_1.0.0_ga.

My codec  is a WM8740 and must be driven by an external clock. IMX can provide this oversampling clock with I2S master mode and SYS_CLK_EN=1.

I'm facing an issue with the fsl_ssi_set_dai_sysclk in fsl_ssi.c which is not calculating correctly the sys clock according to the bitclock requested.

When asking 2822400 which is 44100 * 2 * 32, the sys clock which is calculated is too high(79Mhz instead of 11.2896MHz) as PM (13) for common use of codec such as WM8740. 

wm8740_systemclock.jpg

So i wrote a patch to fix this issue and get acceptable sysc clock.

[Diff] fsl_ssi - Pastebin.com

But concerning higgh frequency such as 192kHz, we are not able to respect this comment as I disabled the check part in the patch.

   The bclk rate must be smaller than 1/5 sysclk rate */

So I would like to confirm first the patch i applied to fsl_ssi.c and understand why this comment in the code and in the IMX6Q's documentation.

rgds.

Stephane

Labels (4)
0 Kudos
7 Replies

382 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Cerveau

this restriction is from IMX6DQRM  sect.61.8.4 SSI Clocking

IMX6DQRM   rev.2.7   7_2014  p.5118.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

382 Views
dabrain
Contributor I

Hello Igor,

Thank you for your answer.

I still dont anwser why its forbidden to have a bitclock greater than 1/5 of the ipg_clk. I have read this caution in documentation.

In my case, in order to get a working 192kHz sample rate, i need 24.576MHz or 36.384MHz (WM8740 Table) as sys clock and 32 *2 * 192000=12,288MHz as bitclock.

So in this case, ipg_clock=24.576MHz and pm=0.

I have been working like this for about a year with previous kernel 3.0.35 without any issues.

Please let me know about the consequences if there are ?

Stephane

0 Kudos

382 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Cerveau

this is forbidden due to processor harwdare design,

that is internal SSI module synchronization is guaranteed provided that

that requirement is fulfiled.

~igor

0 Kudos

382 Views
dabrain
Contributor I

Hi,

I'm not sure to catch you.

Why is it possible to do it software speaking, can it damage the hardware (??)?

Is there some potential jitter issue ?

In my case how can I generate a 192kHz sample rate setup so ?

Best regards.

Stéphane

0 Kudos

382 Views
igorpadykov
NXP TechSupport
NXP TechSupport

SSI hadrware forbids to have a bitclock greater than 1/5 of the ipg_clk.

This is described in RM.

0 Kudos

382 Views
dabrain
Contributor I

Hey Igor,

I read it in the RM too.

I'm sorry to insist but what are the consequences if i dont take this limitation into account?

In table 61.7 in IMX6QDRM.pdf, there is this line where pm is equal to 1 and so bitclk/ssi_sys_clk is equal 1/4 so greater than 1/5

imx6q_pm_44100.png

Thx in advance for your support

0 Kudos

382 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Cerveau

consequences may be that is some

corner PVT cases it may work unpredictable.

table/software comments may be inaccurate, since these

may be left from previous processors docs.

Best regards

igor

0 Kudos