I2C read not being acknowledged - Apple Authentication Co-processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C read not being acknowledged - Apple Authentication Co-processor

Jump to solution
11,569 Views
ruchisirauthiya
Contributor II

Hello,

I am working on iPod Authentication Coprocessor 2.0C (MFI337S3959).

With source code in 'i2c-imx.c', I2C probe and writes are working fine but I2C read is failing. 'i2c_imx_read' is returning after checking for ACK in the function 'i2c_imx_acked'.


We have observed on the scope that for SCL bit-8 (acknowledge), SDA remains low for the read operation and thus there is no acknowledge. Bit-8 for write operation remains low for ACK, which is the correct.

What could be causing read not to be acknowledged? Is there a work around?


Thanks and Regards,

Ruchi

0 Kudos
Reply
1 Solution
6,078 Views
ruchisirauthiya
Contributor II

Solved. Used retry mechanism when NACK is received.

View solution in original post

0 Kudos
Reply
4 Replies
6,078 Views
lavakumars
Contributor IV

hi,

i am also having the apple authentication module trying to use it on imx6qp board ,

but the module is not at all detected . can someone tell how to proceed (#imx6qp) further.

Got the patch from nxp for mfi drivers but no use.:(

Regards,

Lavakumar S

0 Kudos
Reply
6,078 Views
mohammadzahabsh
Contributor I

Hey,

  Can anyone help me as ho to install apple auth chip on imx series boards.

0 Kudos
Reply
6,078 Views
kumarmn
Contributor I

For this same chip I have got the acknowledgement for the slave address but I found NACK for first time i2c_writes & for every i2c_reads.As you said I retried with 500ms delay then I received ACK(for the 2nd retry)  for both i2c_reads & i2c_writes.

I have few queries here,please clarify:

Is this retrying model a fix or only a work around?If there exists a solution kindly let me know.

How many retries were done in your case to get the ACK?

0 Kudos
Reply
6,079 Views
ruchisirauthiya
Contributor II

Solved. Used retry mechanism when NACK is received.

0 Kudos
Reply