I2C iMX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C iMX6DL

980件の閲覧回数
djillaliredjrad
Contributor II

Hi,

I'm trying to use an I2C gyroscope (L3G4200D) on Karo TX6DL (iMX6DL),  I think that the bit start is generated because the IBB bit toggle from 0 to 1, but I don't receive an acknowledge from the slave, when I control scl pin with oscilloscope, I don't find a clock signal.

Where is the problem ?

0 件の賞賛
返信
1 返信

856件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Djillali

it may be recommended to check if SION bit is set in i2c

iomux registers IOMUXC_SW_MUX_CTL_PAD_KEY_X.

Also please check if clock is enabled in CCM_CCGR register.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信