Hello ,
What's issus cause i2c ack too slow as below function?
check my dts file , clock-frequency set 375000 . but receive response still slow.
[ 17.756617] [i2c-core.c][i2c_transfer], line:[2111] i2c_transfer start
[ 17.757515] i2c i2c-0: master_xfer[0] W, addr=0x68, len=1
[ 17.758213] i2c i2c-0: master_xfer[1] R, addr=0x68, len=1
[ 17.805545] [i2c-core.c][i2c_transfer], line:[2134] i2c_transfer done
int i2c_transfer(struct i2c_adapter *adap, struct i2c_msg *msgs, int num)
{
int ret;
/* REVISIT the fault reporting model here is weak:
*
* - When we get an error after receiving N bytes from a slave,
* there is no way to report "N".
*
* - When we get a NAK after transmitting N bytes to a slave,
* there is no way to report "N" ... or to let the master
* continue executing the rest of this combined message, if
* that's the appropriate response.
*
* - When for example "num" is two and we successfully complete
* the first message but get an error part way through the
* second, it's unclear whether that should be reported as
* one (discarding status on the second message) or errno
* (discarding status on the first one).
*/
KDBG("i2c_transfer start");
if (adap->algo->master_xfer) {
//#ifdef DEBUG
for (ret = 0; ret < num; ret++) {
dev_info(&adap->dev, "master_xfer[%d] %c, addr=0x%02x, "
"len=%d%s\n", ret, (msgs[ret].flags & I2C_M_RD)
? 'R' : 'W', msgs[ret].addr, msgs[ret].len,
(msgs[ret].flags & I2C_M_RECV_LEN) ? "+" : "");
}
//#endif
if (in_atomic() || irqs_disabled()) {
ret = i2c_trylock_adapter(adap);
if (!ret)
/* I2C activity is ongoing. */
KDBG("i2c_transfer done");
return -EAGAIN;
} else {
i2c_lock_adapter(adap);
}
ret = __i2c_transfer(adap, msgs, num);
i2c_unlock_adapter(adap);
KDBG("i2c_transfer done");
return ret;
} else {
dev_dbg(&adap->dev, "I2C level transfers not supported\n");
return -EOPNOTSUPP;
}
}
Thanks,
Ben
Solved! Go to Solution.
Hello ben,
You didn't say which processor you are using. But I noticed that the I2C clock is working at 375KHz, so suggest you should check if I2C master and I2C slave device both support Max 400kbps.
In addition, you can set I2C clock to be 100K, then check how about the time of ACK( time of the SDA kept low).
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello ben,
You didn't say which processor you are using. But I noticed that the I2C clock is working at 375KHz, so suggest you should check if I2C master and I2C slave device both support Max 400kbps.
In addition, you can set I2C clock to be 100K, then check how about the time of ACK( time of the SDA kept low).
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------