I2C EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C EEPROM

2,992件の閲覧回数
krishnan_ramesh
Contributor III

Hi,

I am using a 24AA02E64T-I/OT (Microchip) EEPROM and want to interface it with I2C . I am unable to find the driver support for the same in nxp android source.

Would like to know if there's any support available

If yes what are the changes that needs to be done ?

Regards,

Ramesh

ラベル(3)
0 件の賞賛
返信
1 返信

2,870件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ramesh

some examples of i2c eeprom drivers can be found on

eeprom\misc\drivers - linux-imx - i.MX Linux kernel 

at24c dts example

imx6q-h100.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

In general one can look also at examples with spi interface described in Chapter 31 SPI NOR Flash Memory Technology

Device (MTD) Driver attached Linux Manual and Chapter 5 Configuring the SPI NOR Porting Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信