I210 Ethernet Support for IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I210 Ethernet Support for IMX6

1,359件の閲覧回数
ashokp
Contributor I

Hi All,

I am adding the support for I210 intel Ethernet controller support in IMX6 Yocto based BSP. The kernel version is 3.10.31 with device tree support. The I210 device is a PCIe based device. Please let me know if any changes required in dts file to add the support for i210 Ethernet controller. 

Thanks,

P.Ashok

ラベル(6)
0 件の賞賛
1 返信

631件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ashok

i.MX6 PCIe interface is standard inteface, not requiring

additional reconfiguration for every PCIe device, so no need for

changes in dts file.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛