During the development of I.X8DXP platform products, the communication could not be completed in the debugging of THE RGMII interface connection Marvel Switch communication.The switch model is 88E6172.The switch hardware configuration is correct, PHY PORT 0-4 is normal for external communication as the switch, and the RGMII interface cannot be configured successfully. Is there a driver with 88E6172 in I.MX8DXP?
Hi 克祥 黄
for 88E6172 driver one can refer to below links
dsa: mv88e6352/mv88e6xxx: Add support for Marvell 88E6320 and 88E6321 - Patchwork
GitHub - mmilburn/marvell-switch
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear igorpadykov:
Can you provide a complete Linux driver suite and related software migration documentation?Thank you!
one can refer to general linux documentation
https://www.kernel.org/doc/Documentation/networking/switchdev.txt
https://elinux.org/images/8/88/Belloni-Switchdev-Slides-ELC2018.pdf
Best regards
igor
Dear igorpadykov:
At present, i.mx8dxp has received the broadcast network packet, but its IP address cannot be confirmed. Tcpdump - I eth0-v | grep 244 is executed on i.mx8dxp, please see the screenshot.
The configuration instructions used are as follows:
Ping 192.169.5.227 on another COMPUTER on the LAN: 192.169.5.244, the problem is that it cannot confirm its IP address.
Please analyze the reasons and see how to solve them.Thank you very much.
Best regards.
Jack