I would like updated documentation for the IMX6ULL NAND Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I would like updated documentation for the IMX6ULL NAND Boot

Jump to solution
1,504 Views
JohnKlug
Senior Contributor I

I have seen this, and the attachments are no longer valid:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-To-use-NAND-boot-on-i-MX6UL-EVK-boar... 

 

I noticed that this posting references U302 and U303 which are not on current schematics.

 

I am interested in how to configure the current Yocto build for the raw NAND (GPMI) boot.

0 Kudos
Reply
1 Solution
1,490 Views
JohnKlug
Senior Contributor I

Thanks.  I did not realize there was more than one schematic.  I was looking at the board schematic, SPF-28616_C2, and what I needed to look at is SPF-29364_A1.

Also, I see there are instructions for building the NAND boot in section 5.5 of i.MX Yocto Project User's Guide.

 

I think I will start by trying to get the NOR to boot with U-Boot.

 

 

View solution in original post

0 Kudos
Reply
3 Replies
1,491 Views
JohnKlug
Senior Contributor I

Thanks.  I did not realize there was more than one schematic.  I was looking at the board schematic, SPF-28616_C2, and what I needed to look at is SPF-29364_A1.

Also, I see there are instructions for building the NAND boot in section 5.5 of i.MX Yocto Project User's Guide.

 

I think I will start by trying to get the NOR to boot with U-Boot.

 

 

0 Kudos
Reply
1,500 Views
joanxie
NXP TechSupport
NXP TechSupport

do you use imx6ul evk board or imx6ull? which schematic version do you refer to, refer to the cpu schematic you can find U302 and U303

 

0 Kudos
Reply
1,485 Views
JohnKlug
Senior Contributor I

I am using MCIMX6ULL_EVK board and file:

MCIMX6ULL-EVK-DESIGNFILES.zip

which I downloaded from your website.

0 Kudos
Reply