I would like to run a VxWorks 7 image project using the i.MX6 Sabre development board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I would like to run a VxWorks 7 image project using the i.MX6 Sabre development board

1,083件の閲覧回数
paulsayers
Contributor I

The development board is currently using U-Boot 2015.04-00392-g6581aea-dirty (Jul 02 2016 - 14:06:02) and is booting an Android image. I have a simple VxWorks 7 VIP built using the BSP for the i.MX6 Sabre board. The SDCard is formatted for Android OS so how do I get the VxWorks image onto the SD card and how do I boot to this image instead of the Android OS?

0 件の賞賛
返信
1 返信

898件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi paul,

You may need contact Winriver: NXP - Partner Profile Information For that task.

Regards

0 件の賞賛
返信