I would like to amend the dhcp, how to do it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I would like to amend the dhcp, how to do it?

748 Views
qiubin2012
Contributor I

CPU:IMX6S   Kernel:Linux3.0.35  

The board is powered on and configured with static IP. I would like to amend the dhcp, how to do it?

Tags (3)
0 Kudos
Reply
1 Reply

506 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello彬 丘,

You may edit the IP configuration on the kernel boot arguments.

You can see the options available on Table 6 (Kernel Boot Parameters) of the i.MX 6Dual/6Quad SABRE-SD Linux Release Notes.

The parameter would be ip and you can set it to ip = dhcp.

I hope this information helps!

Regards,

0 Kudos
Reply