I want to use SRAM2 with i.MX 8ULP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to use SRAM2 with i.MX 8ULP

Jump to solution
621 Views
daisukemizobuch
Contributor II

hello.

I want to use SRAM2 with i.MX 8ULP, and I want to see how much the power consumption drops.

The function of L2_CACHE_CONTROL in SIM1_SYSCTRL0 is as follows:
0b0 - 256 KB L2 Cache + 256 KB SRAM configuration.
0b1 - 512 KB L2 Cache with no SRAM.

For NXP BSP U-Boot, set it to "0b1".
https://github.com/nxp-imx/uboot-imx/blob/lf-6.1.55-2.2.1/arch/arm/mach-imx/imx8ulp/soc.c#L1008

However, if I comment out this line, the U-Boot SPL will not be able to start U-Boot.

The log is as follows:
U-Boot SPL 2023.04-at2-5-g57cf82d-00005-g31a6c3e2f0-dirty (Jun 26 2025 - 13:08:58 +0900)
Normal Boot
ELE firmware version 1.3.0-c6f74feb
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.18
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories faliure 1, err_code 6, ret_val 0x0
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
drive: OD
SEC0: RNG instantiated
WDT: Started m33-at-wdt with servicing every 1000ms (60s timeout)
Trying to boot from BOOTROM
Boot Stage: Primary boot
image offset 0x0, pagesize 0x200, ivt offset 0x0
Load image from 0x52800 by ROM_API
: (Booting has stopped...)

Is there any other configuration required?

Regards,

mizo

Labels (1)
0 Kudos
Reply
1 Solution
605 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @daisukemizobuch 

You can try rolling back to the code before this commit.

https://github.com/nxp-imx/uboot-imx/commit/610083e547d19e87b567849b299187d66b643fb9


Best Regards,
Zhiming

View solution in original post

0 Kudos
Reply
2 Replies
606 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @daisukemizobuch 

You can try rolling back to the code before this commit.

https://github.com/nxp-imx/uboot-imx/commit/610083e547d19e87b567849b299187d66b643fb9


Best Regards,
Zhiming

0 Kudos
Reply
598 Views
daisukemizobuch
Contributor II

Hi @Zhiming_Liu

Thanks for the reply.

> https://github.com/nxp-imx/uboot-imx/commit/610083e547d19e87b567849b299187d66b643fb9

This commit message gave me a hint and helped me solve the problem!

It became possible to start by reverting the following commit in imx-atf.

https://github.com/nxp-imx/imx-atf/commit/aa50784614c289ee3a468dd247b476327bfd7c76

Best Regards,
mizo

 

0 Kudos
Reply