Status = "disabled" means that the dma function is disabled? I‘m a rookie -_-
uart2: serial@021e8000 { compatible = "fsl,imx6q-uart", "fsl,imx21-uart"; reg = <0x021e8000 0x4000>; interrupts = <0 27 IRQ_TYPE_LEVEL_HIGH>; clocks = <&clks IMX6QDL_CLK_UART_IPG>, <&clks IMX6QDL_CLK_UART_SERIAL>; clock-names = "ipg", "per"; dmas = <&sdma 27 4 0>, <&sdma 28 4 0>; dma-names = "rx", "tx"; status = "disabled"; };