I want to change runlevel 3 to 5 in imx8mp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to change runlevel 3 to 5 in imx8mp

1,272 Views
ankitpanchal167
Contributor III

Hi,

I want to change 3 runlevel  to 5 in imx8mp. 

i try this command with "init 5" but my display not working 

i am also try with "/etc/inittab" file but inittab not working with imx8mp

how to set runlevel as 5 and also woking my display also?

0 Kudos
5 Replies

1,261 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

What runlevel   mean ?Can you give more details about your steps?

0 Kudos

1,256 Views
ankitpanchal167
Contributor III

hi 

runlevel means init rc runlevel like 1 to 6.

i would to change init rc runlevel to 5 

0 Kudos

1,243 Views
ViktorLinnik
Contributor I

You can change runlevel with the command like "/sbin/init 5".

0 Kudos

1,238 Views
ankitpanchal167
Contributor III

Hi Viktor,

Yes, its working this command but after run this command display graphics not working 

0 Kudos

1,223 Views
ViktorLinnik
Contributor I

Please check which scripts are listed in /etc/rc5.d/. These are the scripts running with switching to this runlevel.

0 Kudos