Hello:
I want to boot the Windows CE image from SD card on i.MX53QSB。I use these command to download the device.
cfimager -a -imx53 -d g -f D:\WINCE700\OSDesigns\iMX53_QSB\RelDir\Freescale_i_MX53_QSB_ARMV7_Release\eboot.nb0
cfimager -a -imx53 -d g -f D:\WINCE700\OSDesigns\iMX53_QSB\RelDir\Freescale_i_MX53_QSB_ARMV7_Release\nk.nb0.
--------------------------------
the size of eboot.nb0 is 512kb, the size of NK.nb0 is 149MB.
The following messages are shown but the OS is not started. CE image boot remains the message "Download successful! Jumping to image at 0x0 (physical 0x70200000).". How can I solve this problem?
Thanks!
INFO:OALLogSetZones: dpCurSettings.ulZone
Mask: 0xb
BSP Clock Configuration:
OSC = 24000000 Hz
PLL1 = 800000000 Hz
PLL2 = 600000000 Hz
PLL3 = 400000000 Hz
PLL4 = 595000000 Hz
LP_APM = 24000000 Hz
ARM = 800000000 Hz
AXI_A = 300000000 Hz
AXI_B = 200000000 Hz
EMI_SLOW = 120000000 Hz
AHB = 120000000 Hz
IPG = 60000000 Hz
PERCLK = 8000000 Hz
CKIL_SYNC = 32768 Hz
DDR = 300000000 Hz
ARM_AXI = 200000000 Hz
IPU_HSP = 200000000 Hz
VPU_AXI = 200000000 Hz
GPU = 200000000 Hz
GPU2D = 200000000 Hz
DEBUG_APB = 200000000 Hz
ENFC = 30000000 Hz
USBOH3 = 66666666 Hz
ESDHC1 = 100000000 Hz
ESDHC2 = 100000000 Hz
ESDHC3 = 100000000 Hz
ESDHC4 = 100000000 Hz
UART = 24000000 Hz
SSI1 = 6000000 Hz
SSI2 = 6000000 Hz
SSI3 = 6000000 Hz
SSI_EXT1 = 24000000 Hz
SSI_EXT2 = 19047619 Hz
USB_PHY = 24000000 Hz
TVE_216_54 = 297500000 Hz
DI0 = 50000000 Hz
DI1 = 297500000 Hz
VPU_RCLK = 24000000 Hz
SSI_LP_APM = 24000000 Hz
SPDIF_XTAL = 24000000 Hz
LDB_DIO = 595000000 Hz
LDB_DI1 = 595000000 Hz
SPDIF0 = 1142857 Hz
ESAI = 3000000 Hz
ESAI_HCKR = 0 Hz
ESAI_HCKT = 0 Hz
CAN = 60000000 Hz
FIRI = 24000000 Hz
CSI_MCLK1 = 25000000 Hz
CSI_MCLK2 = 25000000 Hz
ECSPI = 66666666 Hz
LPSR = 0 Hz
PGC = 7500000 Hz
ASRC = 59500000 Hz
IEEE_CEMX = 40000000 Hz
CKIH = 22579200 Hz
CKIH2 = 0 Hz
Microsoft Windows CE Bootloader Common Library Version 1.4 Built May 30 2012 09:25:08 OALMc34708Pmic
I2cInit: Trying to init PMIC I2C Interface
OALPmicInit: Trying to init I2C Interface
MC34708 Version code : 14
INFO: BoardID = 0xc03.
INFO: EVK RevA board is not detected, switch ddr clock to 400MHz.
INFO: Increasing CPU clock to 1.0 GHz.
Microsoft Windows CE Ethernet Bootloader 1.30 for MX53 EVK (May 30 2012 09:29:20)
Get The name for the external PHY is LAN8720
INFO: SBMR = 0x10c63d45.
INFO: Bootloader launched from SD.
ESDHC[1] is being activated...
SD High Density card
SD: Switched to 4 bit mode
INFO: Initialized SD Card
ATA device is not present 0x0
WARNING: OEMPlatformInit: Failed to initialize ATA device.
NAND ID is 0x3f3f3f3f
NAND ID read out is 0x3f3f3f3f, doesn't meet 0xd52c which is expected.
Failed to initialize NandFmd.
WARNING: OEMPlatformInit: Failed to initialize NAND flash device.
SPIFMD_Init: Manufacturer ID = 0x0
SPIFMD_Init: Manufacturer ID is not supported yet
WARNING: OEMPlatformInit: Failed to initialize SPI device.
INFO: Loading boot configuration from SDHC
INFO: Successfully loaded boot configuration from SDHC
System ready! Preparing for download...
Press [ENTER] to launch image stored in SD/MMC or [SPACE] to cancel.
Initiating image launch in 3 seconds.
2 seconds. 1 seconds. 0 seconds.
Launching flash image ...
-BLMenu . INFO: Using device name: 'MX539730'
INFO: Reading NK image to SDHC (please wait)...
INFO: Copying NK image to RAM address 0xa0200000
INFO: Read is 1% complete...
INFO: Read is 100% complete
INFO: Copy of NK completed successfully
Either card is not eSD2.1, or boot partition is not created yet Download successful!
Jumping to image at 0x0 (physical 0x70200000)...