I want down i.mx6q bsp L3.0.35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want down i.mx6q bsp L3.0.35

Jump to solution
930 Views
jhtingjhting
Contributor I

I want down i.mx6q bsp L3.0.35, but can't find it! 

dow new bsp error!!!

/fsl-bsp$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga

gpg: keyring `/home/jht/.repoconfig/gnupg/secring.gpg' created

gpg: keyring `/home/jht/.repoconfig/gnupg/pubring.gpg' created

gpg: /home/jht/.repoconfig/gnupg/trustdb.gpg: trustdb created

gpg: key 920F5C65: public key "Repo Maintainer <repo@android.kernel.org>" imported

gpg: Total number processed: 1

gpg:               imported: 1

Getting repo ...

   from git://android.git.kernel.org/tools/repo.git

android.git.kernel.org[0: 202.96.128.166]: errno=Connection timed out

fatal: unable to connect a socket (Connection timed out)

jht@ubuntu:~/fsl-bsp$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga

Getting repo ...

   from git://android.git.kernel.org/tools/repo.git

android.git.kernel.org[0: 202.96.128.166]: errno=Connection timed out

fatal: unable to connect a socket (Connection timed out)

Labels (1)
0 Kudos
1 Solution
566 Views
himanshugusain
Contributor III

Hi

Use below link to download

i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release

Regards

Himanshu

View solution in original post

0 Kudos
2 Replies
567 Views
himanshugusain
Contributor III

Hi

Use below link to download

i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release

Regards

Himanshu

0 Kudos
566 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The L3.0.35 is not supported more. As for the recent BSP, please
follow exactly recommendations of
“Freescale_Yocto_Project_User's_Guide.pdf”.
In particular - section 
3 (Host Setup).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos