I use i.MX6 DL processor and I tried to set CAN device. However I received the error ip: RTNETLINK answers: Operation not supported Could you help me to add CAN device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I use i.MX6 DL processor and I tried to set CAN device. However I received the error ip: RTNETLINK answers: Operation not supported Could you help me to add CAN device?

1,503 Views
victormazin
Contributor II

I use i.MX6 DL processor and I tried to set CAN device. However I received the error

ip: RTNETLINK answers: Operation not supported      

Could you help me to add CAN device?

root@tx6-dl:~/CanDrivers# ls                                                   

can-bcm.ko  can-dev.ko  can-gw.ko   can-raw.ko  can.ko      flexcan.ko         

root@tx6-dl:~/CanDrivers# modprobe flexcan                                     

root@tx6-dl:~/CanDrivers# modprobe can_raw                                     

root@tx6-dl:~/CanDrivers# modprobe can                                         

root@tx6-dl:~/CanDrivers# ip link add dev can0 type can                        

ip: RTNETLINK answers: Operation not supported                                 

root@tx6-dl:~/CanDrivers# ip link add dev can0 type flexcan                    

ip: RTNETLINK answers: Operation not supported                                 

root@tx6-dl:~/CanDrivers#

Labels (2)
0 Kudos
Reply
4 Replies

925 Views
marcocavallini
Contributor V

Hi Victor,

which kernel version are you using?

What lsmod says after your modprobes ?

--

Marco

0 Kudos
Reply

925 Views
victormazin
Contributor II

 

Hi Marco

Please see below:

 

Linux version 3.12.0-rc6-next-20131024-karo+

   

root@tx6-dl:~/CanDrivers# lsmod                                                
     Not tainted                                                                
w1_gpio 2735 0 - Live 0x7f2bf000                                               
wire 22248 1 w1_gpio, Live 0x7f2b3000                                          
vcan 1954 0 - Live 0x7f2af000                                                  
usbtouchscreen 5379 0 - Live 0x7f2aa000                                        
usbtest 20574 0 - Live 0x7f2a0000                                              
usbserial 24948 0 - Live 0x7f293000                                            
usbmon 17921 0 - Live 0x7f28a000                                               
usbhid 18608 0 - Live 0x7f281000                                               
ums_sddr55 5654 0 - Live 0x7f27c000                                            
ums_sddr09 9547 0 - Live 0x7f276000                                            
ums_realtek 7582 0 - Live 0x7f270000                                           
ums_datafab 5430 0 - Live 0x7f26b000                                           
usb_storage 42463 4 ums_sddr55,ums_sddr09,ums_realtek,ums_datafab, Live 0x7f2570
udf 73831 0 - Live 0x7f23e000                                                  
spi_imx 9502 0 - Live 0x7f237000                                               
spi_gpio 5134 0 - Live 0x7f232000                                              
spi_bitbang 3907 2 spi_imx,spi_gpio, Live 0x7f22e000                           
sparse_keymap 3766 0 - Live 0x7f22a000                                         
snd_soc_imx_audmux 5332 0 - Live 0x7f1cd000                                    
snd_page_alloc 5120 0 - Live 0x7f170000                                        
regmap_spi 1913 0 - Live 0x7f140000                                            
regmap_i2c 1645 0 - Live 0x7f13c000                                            
phy_gpio_vbus_usb 3344 0 - Live 0x7f138000                                     
msdos 6758 0 - Live 0x7f133000                                                 
matrix_keymap 2473 0 - Live 0x7f12f000                                         
libcomposite 36522 0 - Live 0x7f11f000                                         
libahci 26285 0 - Live 0x7f112000                                              
ledtrig_gpio 2950 0 - Live 0x7f10e000                                          
isofs 29506 0 - Live 0x7f102000                                                
i2c_gpio 3220 0 - Live 0x7f0e8000                                              
i2c_dev 5114 0 - Live 0x7f0e3000                                               
gadgetfs 19526 0 - Live 0x7f0da000                                             
udc_core 9156 2 libcomposite,gadgetfs, Live 0x7f0d3000                         
flexcan 9142 0 - Live 0x7f0cd000                                               
ehci_hcd 55793 0 - Live 0x7f0b9000                                             
usbcore 177871 11 usbtouchscreen,usbtest,usbserial,usbmon,usbhid,ums_sddr55,ums0
usb_common 2849 4 usbtest,libcomposite,udc_core,usbcore, Live 0x7f076000       
edt_ft5x06 9089 0 - Live 0x7f06f000                                            
crc_itu_t 1533 1 udf, Live 0x7f06b000                                          
configfs 26751 2 libcomposite, Live 0x7f05e000                                 
can_raw 5987 0 - Live 0x7f059000                                               
can_gw 7699 0 - Live 0x7f054000                                                
can_dev 9544 1 flexcan, Live 0x7f04d000                                        
can_bcm 10732 0 - Live 0x7f01a000                                              
evbug 1881 0 - Live 0x7f016000                                                 
can 23212 3 can_raw,can_gw,can_bcm, Live 0x7f00c000                            
evdev 10143 0 - Live 0x7f005000                                                
tsc2007 4628 0 - Live 0x7f000000                                               
root@tx6-dl:~/CanDrivers#

 

0 Kudos
Reply

925 Views
marcocavallini
Contributor V

Hi Victor,

try following this thread, it works on my side.

https://community.freescale.com/thread/308441

--

Marco Cavallini | KOAN sas | Bergamo - Italia

0 Kudos
Reply

925 Views
victormazin
Contributor II

Hi

I installed a new version of iproute2 package and was able to set up CAN device.

root@tx6-dl:~/Working# ./ip link set up can0 type can  bitrate 20000

flexcan 2094000.flexcan can0: writing ctrl=0xdb29a0d5

flexcan 2094000.flexcan can0: flexcan_set_bittiming: mcr=0x5980000f ctrl=0xdb29a0d5

flexcan 2094000.flexcan can0: flexcan_chip_start: writing mcr=0x79a20208

flexcan 2094000.flexcan can0: flexcan_chip_start: writing ctrl=0xdb29acd5

flexcan 2094000.flexcan can0: flexcan_chip_start: reading mcr=0x69a20208 ctrl=0xdb29acd5

Regards

Victor