I use SN8000 WIFI module,which BSP should I use?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I use SN8000 WIFI module,which BSP should I use?

1,059 次查看
yuanlong
Contributor II

Dear all,

I use SN8000 WIFI module in MCIMX6Q-SDB, which BSP should I use with android 5.02?

标签 (2)
0 项奖励
回复
1 回复

956 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuan

as mentioned below it is supported with Linux 3.14.38

http:/ /wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复