I there any guide for using CAAM as crypto engine in OPTEE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I there any guide for using CAAM as crypto engine in OPTEE

Jump to solution
2,836 Views
jiankang
Contributor III

Dear NXP engineers,

I want to using CAAM as the default crypto engine in OPTEE

is there any guide can help me doing it ?

 

Thanks a lot!

0 Kudos
Reply
1 Solution
2,834 Views
bulat_a
Contributor III
0 Kudos
Reply
4 Replies
2,802 Views
jiankang
Contributor III

hello bulat_a,

For imx8qm serials, does it support CAAM in OPTEE ?

as I checked,  CFG_NXP_CAAM was force set as false...

else ifneq (,$(filter $(PLATFORM_FLAVOR),$(mx8qm-flavorlist)))
$(call force,CFG_MX8QM,y)
$(call force,CFG_ARM64_core,y)
$(call force,CFG_IMX_SNVS,n)
CFG_IMX_LPUART ?= y
CFG_DRAM_BASE ?= 0x80000000
CFG_TEE_CORE_NB_CORE ?= 6
$(call force,CFG_NXP_CAAM,n)
$(call force,CFG_IMX_OCOTP,n)

 

thanks.

0 Kudos
Reply
2,826 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jiankang

 

by default CAAM is used as crypto engine in OPTEE, also may be useful

https://community.nxp.com/t5/i-MX-Processors/How-to-enable-CAAM-accelerating-in-OP-TEE-on-i-MX7-Dual...

 

Best regards
igor

0 Kudos
Reply
2,790 Views
jiankang
Contributor III

hi @igorpadykov

For imx8qm serials, does it support CAAM in OPTEE ?

as I checked,  CFG_NXP_CAAM was force set as false...

else ifneq (,$(filter $(PLATFORM_FLAVOR),$(mx8qm-flavorlist)))
$(call force,CFG_MX8QM,y)
$(call force,CFG_ARM64_core,y)
$(call force,CFG_IMX_SNVS,n)
CFG_IMX_LPUART ?= y
CFG_DRAM_BASE ?= 0x80000000
CFG_TEE_CORE_NB_CORE ?= 6
$(call force,CFG_NXP_CAAM,n)
$(call force,CFG_IMX_OCOTP,n)

 

thanks.

0 Kudos
Reply
2,835 Views
bulat_a
Contributor III
0 Kudos
Reply