Before I begin, may I confirm that apart from I.MX7 duo that is still to be released,
the most powerful Freescale chip that supports ePaper such as eink displays is I.MX6 Dual lite?
I.MX6Dual and I.MX6Dual Plus have no EPDC output to eInk, right?
I would like to switch output between : EPDC eInk screen MIPI DSI to eDP retina panel 2048x1536
Running android 4.2.
Any good Freescale developer boards with Dual lite and EPDC epaper exposed pin interface?
These are some boards I found with I.MX6 Dual Lite but sadly NO EPDC eInk pins exposed?
WandboardDual
RidgeRun Dual lite
Imx6Rex
BoundaryDevices i.mx6
Toradex Colibri
MarS board
I would really appreciate picking up an inexpensive i.mx6 Dual Lite board with EPDC exposed by default, any ideas?
Would it be worth getting a none EPDC board from the list above and then figure out how to expose the EPDC interface of the I.MX6 BGA manually?
In terms of drivers for EPDC interface and MiPi DSI ,where do I get Android 4.2 and Linux drivers?
would appreciate any help, please.
Nikita
Solved! Go to Solution.
Hi Nikita
right, seems i.MX6DL most powerful among supporting EPDC.
i.MX6 Sabre SDP board MCIMX6DL-SDP, spf-27417 connector J506 is EPDC connector.
I am not aware of Android 4.2 drivers, but for Linux one can check
latest BSP, refer to attached Release Notes p.21
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Nikita
right, seems i.MX6DL most powerful among supporting EPDC.
i.MX6 Sabre SDP board MCIMX6DL-SDP, spf-27417 connector J506 is EPDC connector.
I am not aware of Android 4.2 drivers, but for Linux one can check
latest BSP, refer to attached Release Notes p.21
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor. That helps me a lot!
Regarda,
Nikita