目前開發的gateway 是用I.mx280的方案
1) 目前增加了一個通訊模塊是透過usb 接口接到gateway主板上
Hi NXP,
We are working on a gateway with I.mx280 solution.
1) We try to add a communication module via USB interface.
2) In order to install the driver, Kernel needs to add cher device & dynamic module (ko).
3) In order to control the module and its driver, has to add an application at userspace for operating kernel driver & cher device.
Currently, we add dynamic module (ko) in kernel through menuconfig option, but below questions need your support.
a.) Where can modify SDK’s rcS? *We need to know process to modify “SDK rcS init”? (we need “insmod kernel module” when system is boot up)
b.) Where can we add mknod in SDK? *We need to know process to create “character device”? (We want to operate cher device we created in userspace under /dev/.)
c.) where can we add “udev & hotplug rule” in SDK? *We need to know control process of “USB plugged/unplugged”? (in order to has corresponding action in userspace when add/remove.)
Thank you.
which SDK are you using?
Should be the latest one.
Or any way that I can get precise version for you? if it's necessary?
thanks
We have different version of BSP. So I don't know which one you are using.