I'm using the imx8qxp board.I have a few questions about yocto.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I'm using the imx8qxp board.I have a few questions about yocto.

969 次查看
山水之间
Contributor II

I'm using the imx8qxp board.I have a few questions about yocto.

1. How does yocto configure and compile Linux and uboot?Because I didn't see the source code for Linux and uboot.

2. I compiled an sd card image based on i.mx_yocto_project_user 's_Guide, and the uboot phase can run on my board.Now I want to open CONFIG_AHAB_BOOT. How do I do this?

0 项奖励
回复
1 回复

924 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Hagen Fu,

Yocto builds a customized Linux distribution for the i.MX8QXP Board (other NXP boards are also supported by the BSP release, and the Community BSP supports even some third-party boards). This includes the Linux Kernel and Uboot.

However, Yocto fetched the source code on-demand, which is why you won’t find the source code on the sources folders of the Yocto BSP.

For more details on AHAB please check Application Note 12312 (link below):

https://www.nxp.com/docs/en/application-note/AN12312.pdf

I hope this helps!

Regards,

0 项奖励
回复