I'm trying to debug IMX 93 evk on Visual Studio code but doesn't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm trying to debug IMX 93 evk on Visual Studio code but doesn't work

3,367 Views
geb
Contributor III

Hi,

I have some issue with the imx93 evk board, when I'm trying to debug it on VS Code gave me an errore segger GDB serve quit unexpectedly or in th debug console say

warning: could not convert d:\IMX93\mcimx93_evk_blank\hello_world.c from the host encoding (CP1252) to UTF-32. This normally should not happen, please file a bug report.

Program received signal SIGTRAP, Trace/breakpoint trap.

0xdeadbeee in ?? ()

What can I do to resolve this problem?

Thanks

 

 
 
 
 
0 Kudos
Reply
3 Replies

3,335 Views
geb
Contributor III
 
0 Kudos
Reply

3,335 Views
geb
Contributor III

Hi Chavira,

Yes I have downloaded the patch for the J-LINK debugger and put the file on the correct folder but doesn't work

I followed all the support guides that are out there, but none of it works

I'm sendign you the screenshoots

Thanks

0 Kudos
Reply

3,337 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @geb!

Thank you for contacting NXP Support!

 

have you downloaded the patch for the J-LINK debugger?

 

If not please follow the AN14120 

 

Best Regards!

Chavira

0 Kudos
Reply