I'm trying to build YOCTO image and a newbie. While bitbaking the image, I received following errors. Bitbake command: bitbake -k core-image-minimal. How to solve the errors? Do we need to make changes in pkgconfig-native package?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm trying to build YOCTO image and a newbie. While bitbaking the image, I received following errors. Bitbake command: bitbake -k core-image-minimal. How to solve the errors? Do we need to make changes in pkgconfig-native package?

941 Views
snehaljadhav
Contributor II

The following shows the errors seen in the log file.


DEBUG: Executing shell function do_compile
NOTE: make -j 4
make  all-recursive
make[1]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build'
Making all in glib
make[2]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make  all-recursive
make[3]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
Making all in .
make[4]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make[4]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
Making all in m4macros
make[4]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
make  all-am
make[5]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
make[5]: Nothing to be done for `all-am'.
make[5]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
make[4]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
Making all in glib
make[4]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make  all-recursive
make[5]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
Making all in libcharset
make[6]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
make  all-am
make[7]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
make[7]: Nothing to be done for `all-am'.
make[7]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
make[6]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
Making all in .
make[6]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
../x86_64-linux-libtool  --tag=CC   --mode=compile gcc  -DHAVE_CONFIG_H -I. -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I..  -I.. -I../glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib  -DG_LOG_DOMAIN=\"GLib\" -DG_DISABLE_CAST_CHECKS -DGLIB_COMPILATION -DPCRE_STATIC -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -pthread -Wall -Wstrict-prototypes -Werror=declaration-after-statement -Werror=missing-prototypes -Werror=implicit-function-declaration -Werror=pointer-arith -Werror=init-self -Werror=format-security -Werror=format=2 -Werror=missing-include-dirs -fvisibility=hidden -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -O2 -pipe -c -o libglib_2_0_la-gdate.lo `test -f 'gdate.c' || echo '/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/'`gdate.c
x86_64-linux-libtool: compile:  gcc -DHAVE_CONFIG_H -I. -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I.. -I.. -I../glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib -DG_LOG_DOMAIN=\"GLib\" -DG_DISABLE_CAST_CHECKS -DGLIB_COMPILATION -DPCRE_STATIC -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -pthread -Wall -Wstrict-prototypes -Werror=declaration-after-statement -Werror=missing-prototypes -Werror=implicit-function-declaration -Werror=pointer-arith -Werror=init-self -Werror=format-security -Werror=format=2 -Werror=missing-include-dirs -fvisibility=hidden -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -O2 -pipe -c /home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/gdate.c -o libglib_2_0_la-gdate.o
/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/gdate.c: In function 'g_date_strftime':
/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/gdate.c:2497:7: error: format not a string literal, format string not checked [-Werror=format-nonliteral]
       tmplen = strftime (tmpbuf, tmpbufsize, locale_format, &tm);
       ^~~~~~
cc1: some warnings being treated as errors
make[6]: *** [libglib_2_0_la-gdate.lo] Error 1
make[6]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make[5]: *** [all-recursive] Error 1
make[5]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make[4]: *** [all] Error 2
make[4]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make[3]: *** [all-recursive] Error 1
make[3]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make[2]: *** [all] Error 2
make[2]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build'
make: *** [all] Error 2
ERROR: oe_runmake failed
ERROR: Function failed: do_compile (log file is located at /home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/temp/log.do_compile.2368)


Please help me out with this.

Labels (2)
Tags (1)
0 Kudos
2 Replies

638 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Snehal Jadhav,

Would you please provide more details on your configuration? Like for example which BSP or branch you are using, your Host OS and the MACHINE for which you are baking?

It looks like you are using the Community BSP but you didn’t mention which branch. It could be that some packages required for the host are missing.

Regards,

0 Kudos

638 Views
snehaljadhav
Contributor II

Thanks for the reply.

BSP Branch: jethro

Host OS: Ubuntu 14.04

MACHINE: imx6qsabresd

0 Kudos