The following shows the errors seen in the log file.
DEBUG: Executing shell function do_compile
NOTE: make -j 4
make all-recursive
make[1]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build'
Making all in glib
make[2]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make all-recursive
make[3]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
Making all in .
make[4]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make[4]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
Making all in m4macros
make[4]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
make all-am
make[5]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
make[5]: Nothing to be done for `all-am'.
make[5]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
make[4]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/m4macros'
Making all in glib
make[4]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make all-recursive
make[5]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
Making all in libcharset
make[6]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
make all-am
make[7]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
make[7]: Nothing to be done for `all-am'.
make[7]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
make[6]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib/libcharset'
Making all in .
make[6]: Entering directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
../x86_64-linux-libtool --tag=CC --mode=compile gcc -DHAVE_CONFIG_H -I. -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I.. -I.. -I../glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib -DG_LOG_DOMAIN=\"GLib\" -DG_DISABLE_CAST_CHECKS -DGLIB_COMPILATION -DPCRE_STATIC -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -pthread -Wall -Wstrict-prototypes -Werror=declaration-after-statement -Werror=missing-prototypes -Werror=implicit-function-declaration -Werror=pointer-arith -Werror=init-self -Werror=format-security -Werror=format=2 -Werror=missing-include-dirs -fvisibility=hidden -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -O2 -pipe -c -o libglib_2_0_la-gdate.lo `test -f 'gdate.c' || echo '/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/'`gdate.c
x86_64-linux-libtool: compile: gcc -DHAVE_CONFIG_H -I. -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I.. -I.. -I../glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib -I/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib -DG_LOG_DOMAIN=\"GLib\" -DG_DISABLE_CAST_CHECKS -DGLIB_COMPILATION -DPCRE_STATIC -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -pthread -Wall -Wstrict-prototypes -Werror=declaration-after-statement -Werror=missing-prototypes -Werror=implicit-function-declaration -Werror=pointer-arith -Werror=init-self -Werror=format-security -Werror=format=2 -Werror=missing-include-dirs -fvisibility=hidden -isystem/home/debaleena/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/include -O2 -pipe -c /home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/gdate.c -o libglib_2_0_la-gdate.o
/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/gdate.c: In function 'g_date_strftime':
/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/git/glib/glib/gdate.c:2497:7: error: format not a string literal, format string not checked [-Werror=format-nonliteral]
tmplen = strftime (tmpbuf, tmpbufsize, locale_format, &tm);
^~~~~~
cc1: some warnings being treated as errors
make[6]: *** [libglib_2_0_la-gdate.lo] Error 1
make[6]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make[5]: *** [all-recursive] Error 1
make[5]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make[4]: *** [all] Error 2
make[4]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib/glib'
make[3]: *** [all-recursive] Error 1
make[3]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make[2]: *** [all] Error 2
make[2]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build/glib'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/build'
make: *** [all] Error 2
ERROR: oe_runmake failed
ERROR: Function failed: do_compile (log file is located at /home/debaleena/fsl-community-bsp/build/tmp/work/x86_64-linux/pkgconfig-native/0.28+gitAUTOINC+40342dd0ea-r0/temp/log.do_compile.2368)
Please help me out with this.
Hello Snehal Jadhav,
Would you please provide more details on your configuration? Like for example which BSP or branch you are using, your Host OS and the MACHINE for which you are baking?
It looks like you are using the Community BSP but you didn’t mention which branch. It could be that some packages required for the host are missing.
Regards,
Thanks for the reply.
BSP Branch: jethro
Host OS: Ubuntu 14.04
MACHINE: imx6qsabresd