I have a reboot issue on imx8m Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have a reboot issue on imx8m Mini

477 Views
jack-6602
Contributor I

Dear NXP Support Team:

I'm working on imx8m mini board, the uboot version is 2023.01, kernel version is 6.6.58. Debian12

1: Plug USB keyboard into USB host of main board.

2: power on and press the shortcut key Ctrl+Alt+Del at the same time. (Keep pressing the release shortcut key, not holding it down and not letting go)

Expect results:

System booting normal even if press the shortcut key Ctrl+Alt+Del

Actual results:

System will be rebooted during press the shortcut key.

Actually, I have alreadly configured in system.

1: CtrlAltDelBurstAction=none

2: HandleRebootKey=ignore

3: HandlePowerKey=ignore

4: HandleSuspendKey=ignore

 

The following is log:

U-Boot SPL 2023.01+dfsg-2+exp2-00021-gc17db9adfe-dirty (Feb 13 2025 - 06:40:59 +0000)
WDT: Started watchdog@30280000 with servicing every 1000ms (60s timeout)
NOTICE: Do not release JR0 to NS as it can be used by HAB
NOTICE: BL31: v2.8(debug):c433a63
NOTICE: BL31: Built : 16:00:56, Jan 30 2024
INFO: GICv3 with legacy support detected.
INFO: ARM GICv3 driver initialized in EL3
INFO: Maximum SPI INTID supported: 159
INFO: BL31: Initializing runtime services
INFO: BL31: cortex_a53: CPU workaround for 855873 was applied
WARNING: BL31: cortex_a53: CPU workaround for 1530924 was missing!
INFO: BL31: Preparing for EL3 exit to normal world
INFO: Entry point address = 0x40200000
INFO: SPSR = 0x3c9


U-Boot 2023.01+dfsg-2+exp2-00021-gc17db9adfe-dirty (Feb 13 2025 - 06:40:59 +0000)

CPU: Freescale i.MX8MMQ rev1.0 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 51C
Reset cause: POR
DRAM: 2 GiB
Core: 233 devices, 26 uclasses, devicetree: separate
WDT: Started watchdog@30280000 with servicing every 1000ms (60s timeout)
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... OK
[ 0.000000] KASLR disabled due to lack of seed
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 1.179756] samsung-dsim 32e10000.dsi: supply vddcore not found, using dummy regulator
[ 1.187889] samsung-dsim 32e10000.dsi: supply vddio not found, using dummy regulator
[ 1.219728] spi-nor spi3.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00
[ 1.290995] failed to register cpuidle driver

[ 1.692248] ### ds90ub941_atomic_enable
Loading, please wait...
Starting systemd-udevd version 252.33-1~deb12u1
Begin: Loading essential drivers ... done.
Begin: Running /scripts/init-premount ... done.
Begin: Mounting root file system ... Begin: Running /scripts/local-top ... done.
Begin: Running /scripts/local-premount ... done.
Warning: fsck not present, so skipping root file system
done.
Begin: Running /scripts/local-bottom ... done.
Begin: Running /scripts/init-bottom ... [ 3.831971] ### ds90ub941_atomic_disable
[ 3.876033] imx2-wdt 30280000.watchdog: Device shutdown.
[ 3.881567] reboot: Restarting system

 

Could you give some idea or how to debug to check which part trigger the watch dog?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

470 Views
jack-6602
Contributor I

CtrlAltDelBurstAction=none This configuration can solve the problem that pressing the shortcut key Ctrl+Alt+Del will not restart the system after the system starts, which is valid.

However, if the shortcut key Ctrl+Alt+Del is pressed during kernel startup, the system will restart, and this configuration will be invalid.

0 Kudos
Reply