I cant stop Watchdog - iMX6

cancel
Showing results for 
Search instead for 
Did you mean: 

I cant stop Watchdog - iMX6

1,183 Views
karthikeyanraju
Contributor III

Hi all,

I am using Yocto bsp version 4.1.15_2.0.0 . I have enabled watchdog in u-boot. I am trying to stop the watchdog from filesystem using application.  I have already done the below tests,

Using application - ioctl functions like alive ,watchdog discard and closing the watchdog

Using memtool  -  Extending the WD time in register, but it did not worked . Can anyone help me to solve this issue ?

Labels (2)
0 Kudos
2 Replies

283 Views
karthikeyanraju
Contributor III

Hi igorpadykov,

Thanks for your quick response.

Is there any way to make u-boot watchdog alive ? I have tried watchdog apis to keep alive using application, But doesnt worked. I want to keep my watchdog alive...  Can you give suggestion.

0 Kudos

283 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Karthikeyan 

once started, watchdog can not be disabled as some bits like WDE Watchdog Enable,

are write one once only bits. This is described in sect.70.7.1 Watchdog Control Register

(WDOGx_WCR) i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------