I cannot build U-Boot imx_v2018.03_4.14.98_2.0.0_ga

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I cannot build U-Boot imx_v2018.03_4.14.98_2.0.0_ga

2,518件の閲覧回数
duliguang
Contributor I

I can successfully compile the kernel in a standalone environment, but I cannot build U-Boot imx v2018.03_4.14.98_2.0.0_ga

1、source /opt/fsl-imx-fb/4.14-sumo/environment-setup-aarch64-poky-linux

2、 export ARCH=arm64

3、 cd uboot-imx

4、 make clean

5、make imx8qxp_mek_defconfig

6、 make u-boot.imx

make[2]: “arch/arm/dts/fsl-imx8qxp-mek.dtb”已是最新。
SHIPPED dts/dt.dtb
FDTGREP dts/dt-spl.dtb
CAT u-boot-dtb.bin
COPY u-boot.bin
CFGS .cfgtmp
aarch64-poky-linux-gcc: error: FORCE: No such file or directory
aarch64-poky-linux-gcc: warning: ‘-x c’ after last input file has no effect
aarch64-poky-linux-gcc: fatal error: no input files
compilation terminated.
arch/arm/mach-imx/Makefile:99: recipe for target '.cfgtmp' failed
make[1]: *** [.cfgtmp] Error 1
Makefile:912: recipe for target 'u-boot.imx' failed
make: *** [u-boot.imx] Error 2

see attached:uboot-imx/arch/arm/mach-imx/Makefile

What is the possible cause?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,354件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Du lg,

Is the problem still present? The following threads may also be helpful:

https://community.nxp.com/docs/DOC-328584

https://community.nxp.com/thread/452627

I hope this helps!

Regards,

0 件の賞賛
返信

2,354件の閲覧回数
petersonhou
Contributor II

hello gusarambula,

i download the uboot-imx with git clone uboot-imx - i.MX U-Boot and git checkout -b rel_imx_4.14.98.2.3.0

when i "ls configs"

there is no "imx8qxp_mek_defconfig" at all

am i cloning wrong address or something in git operation?

0 件の賞賛
返信

2,353件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi duliguang@brisonus.com ,

Please use only "make" in step 6. For generating standalone image other imx images, please refer to section 4.5.12 and 4.5.13 from the attached "i.MX Linux User Guide".

Let us know if you face any issue.

Regards,

Radhika

0 件の賞賛
返信