I can't change the CPU frequency on the fly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't change the CPU frequency on the fly

1,090 Views
alex
Contributor I

Hi all:

  I can't change the CPU frequency on the fly on mx28evk board, and in the Reference Manual document it tells us it is OK.

Labels (1)
0 Kudos
Reply
1 Reply

857 Views
YS
Contributor IV

I have same problem here either. It seems like iMX28 Linux cpufreq driver

has serious bug.

The reference manual says

echo 392727 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed

will change the CPU frequency, but the board just locks up.

(392727 should not be a supported frequency for iMX28 -

cat /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state shows

261818, 360000 and 454736 as supported frequency. Anyway, setting

other than 454736 to scaling_setspeed causes lock-up).

My EVK is iMX28 EVK Rev.D, using Linux SDHC memory came with the EVK; uname -a shows

Linux freescale 2.6.31-855-ge067785 #1 Fri Sep 10 09:22:06 MDT 2010 armv5tejl GNU/Linux

Google search shows same issue was reported on forum back on Jul 2011.

http://imxcommunity.org/forum/topics/imx28-change-the-cpu?commentId=4103961%3AComment%3A34105&xg_sou...

Even though patch is provided from Freescale, it was reported it didn't fix the problem.

0 Kudos
Reply