I have a custom imx8mn board, im trying to get the sdcard to work. I can see it in u-boot but it wont probe in linux.
Any ideas?
解決済! 解決策の投稿を見る。
Would suggest check the DTS and Driver. Refer to the usdhc2 node of 8mn (linux-imx/imx8mm-evk.dtsi at lf-6.1.y · nxp-imx/linux-imx · GitHub) and these CONFIG_MMC, CONFIG_MMC_BLOCK, CONFIG_EXT4_FS enabled or not.
If there is /dev/mmcblk1 node, then check its driver.
Best regards
Harvey
Would suggest check the DTS and Driver. Refer to the usdhc2 node of 8mn (linux-imx/imx8mm-evk.dtsi at lf-6.1.y · nxp-imx/linux-imx · GitHub) and these CONFIG_MMC, CONFIG_MMC_BLOCK, CONFIG_EXT4_FS enabled or not.
If there is /dev/mmcblk1 node, then check its driver.
Best regards
Harvey