I am trying to select a processor for my application. I have came across IMX7 solo processor which can be the best processor for my application. When I intended to check the pin mux of the processor using "Pins for IMX version 3.0", I cannot find the IMX7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am trying to select a processor for my application. I have came across IMX7 solo processor which can be the best processor for my application. When I intended to check the pin mux of the processor using "Pins for IMX version 3.0", I cannot find the IMX7

1,653件の閲覧回数
deepanchakravar
Contributor I

I am trying to select a processor for my application. I have came across IMX7 solo processor which can be the best processor for my application. When I intended to check the pin mux of the processor using "Pins for IMX version 3.0", I cannot find the IMX7 series in the processor selection window. In the Software main web page it is mentioned that the IMX7S is supported by the tool.But I cant find the IMX7 in the new configuration window after installed. Only IMX6 Quad is available in the list. Kindly suggest me the way to check the pinmux for my processor.

0 件の賞賛
返信
1 返信

1,606件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi,

the pinstool support i.MX7D, pleae download latest version which is 3.0.2.

Pins Tool for i.MX Application Processors|NXP 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信