/freeglut-3.2.1# cmake . -DFREEGLUT_WAYLAND=ON
CMake Error at /usr/share/cmake-3.13/Modules/FindPackageHandleStandardArgs.cmak:
Could NOT find OpenGL (missing: OPENGL_opengl_LIBRARY OPENGL_glx_LIBRARY
OPENGL_INCLUDE_DIR)
Call Stack (most recent call first):
/usr/share/cmake-3.13/Modules/FindPackageHandleStandardArgs.cmake:378 (_FPHSA)
/usr/share/cmake-3.13/Modules/FindOpenGL.cmake:395 (FIND_PACKAGE_HANDLE_STAND)
CMakeLists.txt:262 (FIND_PACKAGE)...
This is directly trying to install on board with cmake command.
Board: imx8qxp [4.14.78x]
compiled with thsi command:
bitbake fsl-image-qt5
In case unavailability let me know how to add feature like: libmesa-dev, mesa-common-dev, libglu1-mesa-dev, freeglut3-dev, python3-openGL......
Solved! Go to Solution.
Hello Sandeep,
Opengl is available by default in MX8QXP, You need to find the freeglut that are for 64bit libraries.
regards
Can you Plese provide some refrence for adding free-glut to add with yocto with full functionality. i found that glut shared binaries are avaialable at /usr/lib but there is no glut-devel present means headers file are missed [I took installed those headers manually and successfuly compiled].
I have also faced a run time error such as freeglut ( ): OpenGL GLX extension not supported by display ':0'....
how to resolve above issue....If there is some steps missed could you please let me know the right steps to be resolved with refrences or steps....?
Hello Sandeep,
Opengl is available by default in MX8QXP, You need to find the freeglut that are for 64bit libraries.
regards
Along with That Can you please share the way how to download Vivante...Tool Kit.
Does Vivante tool-kit Internally support feature of opengl and opencv?